Hi,
I would like to understand more detail in AD9781 LVDS.
In AD9781 datasheet, LVDS inputs with dual-port or optional interleaved single-port operation:
Might I know if ADI have more detail regarding to 2 different port operation? Such as Timing diagram.
We have two different set of input and output.
I assume the following is the interleaved single-port.
Might I know how is the dual-port operation? AD9781 only has D13-D0 data pin.
I am not sure if AD9781 can be dual port input in parallel.
Please kindly advise. Appreciate your help in advance.
Mark