Hi,
I'm trying to evaluate the AD9783 (on the AD9783-DPG2-EBZ eval board) for my current development project.
Unfortunately the USB Drivers aren't installed correctly.
When I connect the usb cable to my PC the device manager shows an Error Code 28 (The drivers for this device are not installed.)
I have ACE 1.23.3085.1388 and the AD9783-DPG2-EBZ 1.2019.43200 plugin installed.
No hardware is being displayed as attached, when I manually select the hardware it constantly shows a Reset failed message.
From another post in the forum I installed the (probably now) outdated DAC Software Suite.
Now at least a driver is present but I also cannot alter the settings of the dac board with the 978X.vi application. (the check boxes revert to their default settings.
Can you help me with those issues?
Kind regards,
Robert