Post Go back to editing

AD9106 / AD9102 - Dout

Thread Summary

The user is experiencing an issue with the DOUT signal duration on the AD9106, which is much longer than expected. The final answer suggests that the DOUT_MODE bit should be set to 1 for DOUT to depend on DOUT_START and DOUT_STOP delays, and to ensure the pattern repeats only the non-zero part of the signal. The user has confirmed that the DOUT signal is now updating correctly but remains too long. The support team is working on providing a sample code for 3-wire SPI communication to further assist with the issue.
AI Generated Content

Hello,

I try to use DOUT on the AD9106.

I managed to change Dout's state, however the duration is much longer than expected.

I would expect Dout to go back to 0 at the end of the pattern.

Is there a register to reduce Dout duration ?

Best regards,

Marc

Parents
  • I represented when we would expect the end of Dout by arrow.

    Best regards,

    Marc

  • Hello,

    Try changing the DOUT_START_DELAY register value. Here are the registers related to DOUT. Default value is the minimum register value.



    More details about DOUT in page 27 of the datasheet.

    Regards,
    Shine

  • Hello Shine !

    This register slightly increases the duration of Dout (as expected) but still not what we need.

    The pattern generator seems to turn off a long time after the pattern end.

    Do you have a screenshot where the Dout signal last exactly the duration of the pattern ?

    Best regards,

    Marc

  • Hello ,

    Hope you are safe and well. 

    Have you tried adjusting the PATTERN_PERIOD? It should be equal to the number of SRAM addresses used for the waveform multiplied by clock period.

    You can also try raising the edge of the trigger pin or writing  0 to RUN bit 0x1E [0]. The  pattern generation only stops at the end of the current pattern period.

    Thanks, 

    Lorenz

  • Hello Lorenz,

    I took screenshots to get Dout signal duration when the pattern period equals to 4096.

    Almost 7ms ! while the useful signal lasts only for ~30 µs

    And when the pattern period equals 2048. About 3.5ms.

    Now with a zoom on the signal:

    PATTERN_PERIOD = 4096

    PATTERN_PERIOD = 2048

    This register reduces the duration of Dout but it is still far too long.

    Here are the registers values:

    a1 E00
    a2 0
    a3 10
    a4 0
    a5 0
    a6 0
    a7 0
    a8 0
    a9 1F0A
    aA 1F0A
    aB 1F0A
    aC 1F0A
    aD 0
    aE 4000
    aF 0
    a10 0
    a11 0
    a12 0
    a13 0
    a14 0
    a15 0
    a16 0
    a17 0
    a18 0
    a19 0
    a1A 0
    a1B 0
    a1C 0
    a1D 0
    a1E 1
    a1F 1
    a20 E
    a21 0
    a22 0
    a23 0
    a24 0
    a25 0
    a26 101
    a27 0
    a28 111
    a29 1000
    a2A 101
    a2B 1
    a2C 3
    a2D 0
    a2E 0
    a2F 0
    a30 0
    a31 0
    a32 0
    a33 0
    a34 0
    a35 7FF0
    a36 1
    a37 200
    a38 0
    a39 0
    a3A 0
    a3B 0
    a3C 0
    a3D 0
    a3E 0
    a3F 0
    a40 0
    a41 0
    a42 0
    a43 0
    a44 0
    a45 0
    a46 0
    a47 0
    a48 0
    a49 0
    a4A 0
    a4B 0
    a4C 0
    a4D 0
    a4E 0
    a4F 0
    a50 0
    a51 FFF0
    a52 FFF0
    a53 100
    a54 0
    a55 FFF0
    a56 FFF0
    a57 100
    a58 0
    a59 FFF0
    a5A FFF0
    a5B 100
    a5C 0
    a5D 0
    a5E FFF0
    a5F 100
    a60 0
    a61 0
    a62 0
    a63 0
    a64 0
    a65 0
    a66 0
    a67 0
    a68 0
    a69 0
    a6A 0
    a6B 0
    a6C 0
    a6D 0
    a6E 0
    a6F 0
    a70 0
    a71 0
    a72 0
    a73 0
    a74 0
    a75 0
    a76 0
    a77 0
    a78 0
    a79 0
    a7A 0
    a7B 0
    a7C 0
    a7D 0
    a7E 0

     

  • Thank you  for addressing Marc's concern.


    Hi ,

    Lorenz' suggestions are all correct. We just forgot to emphasize that if you want DOUT to depend on DOUT_START and DOUT_STOP values, DOUT_MODE bit should be 1. Otherwise, DOUT will be controlled manually and it will wait for DOUT_VAL bit to be toggled before it changes state. In your waveform captures, the time that DOUT changed state might be right before the next pattern period is played hence the long duration.

    Moreover, you are showing channel 1 output right? If yes, the readback values of registers related to channel 1 are as follows:
    0x29 PAT_PERIOD:     0x1000 - 4096 clock cycles
    0x45 DDSx_CONFIG:  0x0000 - bit 2 DDS_MSB_EN1 is 0 hence SRAM address is incremented every DAC clock cycle
    0x5D START_ADDR1: 0x0000 - DAC1 starts to read waveform from SRAM address 0x6000
    0x5E STOP_ADDR1:   0xFFF0 - DAC1 stops to read waveform at SRAM address 0x6FFF

    This means that the pattern repeats every 4096*clock period (seconds) and the DDS waveform is modulated by the values stored across all the SRAM addresses. So when you repeat the pattern, there are flat parts aside from the "useful" signal. This is because if you are using example 5 SRAM vector, only ~30us ÷ your DAC clock period SRAM addresses are non-zero. See config.h.

    So if you want only the non-zero part of the signal to repeat, follow Lorenz' recommendation with regards to the START_ADDR, STOP_ADDR, and PAT_PERIOD registers.


    Regards,
    Shine

  • Hello Shine,

    Thank you very much for your help.

    So concerning DOUT, I disabled Dout Mode to be able to read the registers since Dout is mutiplexed with SDO. This is why you saw it disabled in the registers.

    Here is what I do to enable/disable DoutMode:

    void AD910xDoutMode(Uint16 state) // Ok?
    {
    	writeDDS(PAT_STATUS, 0);
    	// Enabling Dout implies to switch to SPI3WIRE
    	ShallowSPIConfig.bits.SPI3WIRE = state&1;
    	ShallowSPIConfig.bits.SPI3WIREM = state&1;
    	ShallowSPIConfig.bits.SPI_DRV = state&1;
    	ShallowSPIConfig.bits.SPI_DRVM = state&1;
    	ShallowSPIConfig.bits.DOUT_EN = state&1;
    	ShallowSPIConfig.bits.DOUT_ENM = state&1;
    	writeDDS(SPICONFIG, ShallowSPIConfig.all);
    
    	writeDDS(RAMUPDATE, 1);    // update RAM
    	writeDDS(PAT_STATUS, 1);
    
    	DELAY_US(10);
    
    	writeDDS(PAT_STATUS, 0);
    	ShallowDoutConfig.bits.DOUT_MODE = state&1;
    	writeDDS(DOUT_CONFIG, ShallowDoutConfig.all);
    
    	writeDDS(RAMUPDATE, 1);    // update RAM
    	writeDDS(PAT_STATUS, 1);
    }

    Strangely I have to do this twice to get Dout working.

    Then I can change DoutStartDelay or DoutStopDelay which has an effect. I don't think it is in manual mode.

    Does the start and stop delay work in manual mode too ?

    Concerning PAT_PERIOD and START_ADDR, STOP_ADDR, I not sure to fully understand what you mean : PAT_PERIOD = 4096 and START_ADDR = 0x0, STOP_ADDR  = 0xFFF so it is seems consistent to me.

    This means that the pattern repeats every 4096*clock period (seconds) and the DDS waveform is modulated by the values stored across all the SRAM addresses. So when you repeat the pattern, there are flat parts aside from the "useful" signal. This is because if you are using example 5 SRAM vector, only ~30us ÷ your DAC clock period SRAM addresses are non-zero. See config.h.

    The DDS is not used here, and there is not modulation by SRAM, I send the data in RAM directly. Here you can see with a parabolic curve repeated 4 times:

    Honestly, everything else works very well including DDS (sine) mode. Only Dout is too long.

    Do you have a complete list of registers with the use of Dout so I can try to match them on my board ?

  • Hi Marc,

    Strangely I have to do this twice to get Dout working.

    You need to write on the PAT_STATUS bit first before setting the RAMUPDATE bit. Maybe that's why you need to go through your code twice to enable DOUT.

    Does the start and stop delay work in manual mode too ?

    No.

    Otherwise, DOUT will be controlled manually and it will wait for DOUT_VAL bit to be toggled before it changes state.

    Do you have a complete list of registers with the use of Dout so I can try to match them on my board ?

    Unfortunately we only have code for 4-wire SPI mode.

    In the waveform you sent below, you're using all 4096 SRAM addresses?

    The DDS is not used here, and there is not modulation by SRAM, I send the data in RAM directly. Here you can see with a parabolic curve repeated 4 times:


    Regards,
    Shine

  • Hello Shine,

    Yes the signals were using all 4096 SRAM addresses in the screenshots. And we are only using the channel 1.

    So we read as much points as in PATTERN PERIOD.

    Only Dout is too long now. I can update the registers correctly immediately now.

    Let me know if you have any suggestion.

    Regards,

    Marc

  • Hello,

    Do you have any new idea to try ?

    This problem prevents us from using the component on our new product which is unfortunate since it covers  all the other needs.

    Best regards,

    Marc

  • Hi Marc,

    We are trying to implement 3-wire SPI communication using the EvB so we can provide you with a sample code.

    Regards,
    Shine

  • Hello Shine,

    Have you got any news about this sample code ?

    Best regards,

    Marc

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.