Post Go back to editing

The thickness of the AD9163 package

Hello,

I have a question from our customer about the thickness of the AD9163 package.
The maximum height from the bottom of the ball to the top of the package is 0.95mm which is described in the figure-141 of the datasheet.
This customer wants to know whether he can assume the maximum thickness of the package can be calculated by subtracting the maximum ball height(0.36mm) from the maximum height of the package included the ball height, 0.95mm.


Is this understanding true?

Best regards,

y_suzuki