Post Go back to editing

EVAL-AD9121 and ADS7-V2EBZ

Thread Summary

The user inquires about evaluating the AD9121 DAC with either ADS7-V2EBZ or SDP-H1. The final answer confirms that AD9121 can be evaluated with the SDP-H1, but the ADS7-V2EBZ is required for the AD9680 ADC. The user seeks to minimize board preparation costs and centralize support, but the AD9121 is not listed on the ADS7-V2EBZ product page, raising concerns about compatibility and future support.
AI Generated Content

Hello

I have one question. please tell me.

I'm considering the AD9121 as an evaluation board that meets the specifications below.

 ・Out put channels :2ch

 ・Update Rate:1Gsps

 ・Resolution :14bit

 ・output Range:1Vp-p(50Ω)

Should I prepare the following evaluation board?

 case1:AD9121-M5375-EBZ and AD-DAC-FMC-ADP and ADS7-V2EBZ

 case2:AD9121-M5375-EBZ and AD-DAC-FMC-ADP and EVAL-SDP-CH1Z

Is it possible to evaluate AD9121 in either case1 or case2?

Please let me know if there is something missing in the evaluation..

Best Regards.