Post Go back to editing

EVAL-AD9121 and ADS7-V2EBZ

Thread Summary

The user inquires about evaluating the AD9121 DAC with either ADS7-V2EBZ or SDP-H1. The final answer confirms that AD9121 can be evaluated with the SDP-H1, but the ADS7-V2EBZ is required for the AD9680 ADC. The user seeks to minimize board preparation costs and centralize support, but the AD9121 is not listed on the ADS7-V2EBZ product page, raising concerns about compatibility and future support.
AI Generated Content

Hello

I have one question. please tell me.

I'm considering the AD9121 as an evaluation board that meets the specifications below.

 ・Out put channels :2ch

 ・Update Rate:1Gsps

 ・Resolution :14bit

 ・output Range:1Vp-p(50Ω)

Should I prepare the following evaluation board?

 case1:AD9121-M5375-EBZ and AD-DAC-FMC-ADP and ADS7-V2EBZ

 case2:AD9121-M5375-EBZ and AD-DAC-FMC-ADP and EVAL-SDP-CH1Z

Is it possible to evaluate AD9121 in either case1 or case2?

Please let me know if there is something missing in the evaluation..

Best Regards.

Parents Reply Children
No Data