Post Go back to editing

EVAL-AD9121 and ADS7-V2EBZ

Hello

I have one question. please tell me.

I'm considering the AD9121 as an evaluation board that meets the specifications below.

 ・Out put channels :2ch

 ・Update Rate:1Gsps

 ・Resolution :14bit

 ・output Range:1Vp-p(50Ω)

Should I prepare the following evaluation board?

 case1:AD9121-M5375-EBZ and AD-DAC-FMC-ADP and ADS7-V2EBZ

 case2:AD9121-M5375-EBZ and AD-DAC-FMC-ADP and EVAL-SDP-CH1Z

Is it possible to evaluate AD9121 in either case1 or case2?

Please let me know if there is something missing in the evaluation..

Best Regards.

Parents Reply Children
  • Hi Patrick-Xuan

    I'm sorry, but my explanation was inadequate, so let me supplement it.
    As a background to this question, customers are considering not only DAC: AD9121 but also ADC: AD9680.
    Therefore, ADS7-V2EBZ is required to operate EVAL-AD9680.

    I understand that the AD9121 can be evaluated with "SDP-H1", but if possible, I would like to combine the boards used for evaluation into one.
    The reason is that we want to keep board preparation costs down and put together support.
    Therefore, I was constantly asking if the AD9121 could work with the ADS7.

    Again, would you recommend using the AD9121 with the SDP-H1?
    If possible, I would like information on whether it can be used as a set with ADS7.
    Also, could you provide guidance on how to get ADS7 to work if available?

    Best Regards.

  • Hi Baggio, 

     AD9121 can be supported by ADS7-V2,   pls use  the latest  DPG Lite, which is included in the ACE installation package. 

    Best regards

  • Hi Patrick-Xuan-san.Thank you for your answer.

    I appreciate your help.

    Best regards