Post Go back to editing

AD9961 unused pins?

Is there any termination advice for unused pins on the AD9961/3?

For example, I'm planning on only using half duplex mode--can I leave TXD[0:9] unconnected?

Can I leave AUX33V unconnected if I'm not planning on using the AUX ADCs?

Thanks!

  • Hello,

    Suggest that you tie TXD11 to TXD0 TxDAC Input Data (pins 39 to 50) to GND by 1st connection all pins together and then using 1 kohm resistor to connect this node to GND.  With regard to AUX33V..........suggest that you still apply 3.3 V supply to it.