I am trying to setup the AD9163 board. I made a following setting sequence refering to start up sequence. And add the CDR reset of updated start-up sequence.
but didn't go well.
I tried to check address 0x31E PHY_DATA_SNAPSHOT function,but the snapped data is always 0x00.
I checked the serdes input lane by oscilloscope,the somthing signal was comming . but no validation checked.
I think irresponsible value was snapped if the input signal is wrong.
Would you help me if these setting is ok ?
Thanks.
#-------------------------------------
# Fdac=4800M
# L=8/Interpolate=6
# LaneRate=4Gbps
# SYSREF CLK is 1MHz pulse , but not used
#-------------------------------------
w,0000,18
w,00D2,52
w,00D2,D2
w,0606,02
w,0607,00
w,0604,01
r,0003 ---> 0x04
r,0004 ---> 0x63
r,0005 ---> 0x91
r,0006 ----> 0x03
r,0604 ----> 0x62
w,0058,03
w,0090,1E
w,0080,00
w,0040,00
w,009E,85
w,0091,E1
#--0092: DLL Status
r,0092 ----> 0x01
w,00E8,20
w,0152,00
#---------------------------------------
# JESD setings
# 4Gbps: 0x084[5:4]=00/0x289[1:0]=01
#---------------------------------------
w,0300,00
w,04B8,FF
w,04B9,01
w,0480,38
w,0481,38
w,0482,38
w,0483,38
w,0484,38
w,0485,38
w,0486,38
w,0487,38
#-- 0x0334: Lane Invert
w,0334,00
#-- 0x0110: Lane/Interpolate
w,0110,84
w,0111,00
w,0230,00
w,0289,01
w,0084,00
w,0200,00
#--0x475(3): QBD reset on
w,0475,09
#-- 0x0453(7): Descramble on
w,0453,80
w,0458,0F
w,0459,21
#--0x475(3): QBD reset off
w,0475,01
w,0201,00
w,02A7,01
w,02AE,01
w,029E,1F
#-- 0x0206: CDR
w,0206,00
w,0206,01
#-- 0x0280: Serdes PLL
w,0280,01
#--0281: PLL Status
r,0281 ---> 0x0b
#--0300: Enable Serdes
w,0300,01
r,0470 ----> 0x00
r,0471 ----> 0x00
r,0472 ----> 0x00
r,0473 ----> 0x00
-------------------------------------------
#-- 0x0206: CDR
w,0206,00
w,0206,01
#--grab phy recv data
w,031E,1D
w,031E,1C
r,031F ----> 0x00
r,0320 ----> 0x00
r,0321 ----> 0x00
r,0322 ----> 0x00
r,0323 ----> 0x00