Post Go back to editing

LTC2000 DAC Clock Driver

Thread Summary

The user inquires about using the ADN4650 as a DAC Clock Driver IC for the LTC2000, operating at CKP/N=200MHz and DCKIP/N=100MHz. The support engineer confirms that the ADN4650's 250mV |Vod| min is 50mV below the LTC2000's 300mV differential input voltage min, but suggests increasing the output load resistance from 100Ω to 120Ω to meet the requirement. The user will follow up with the ADN4650 team.
AI Generated Content

Hi

I am FAE in Japanese Distributor.

Our customer will use LTC2000 at CKP/N=200MHz and DCKIP/N=100MHz

Figure 13 shows DAC Clock with the LTC6946.

But RF output frequency of  LTC6946 is from 370MHz to 6.39GHz.

He thinks to use ADN4650 as  DAC Clock Driver IC.

Does ADN4650 work well the following circuit?

Could you recommend other DAC Clock Driver IC?

Best regards

N.Kokubo

Parents Reply Children