Post Go back to editing

AD9174 with ADS7-V2 example setup help

I am currently attempting to set up the AD9174 eval board with the ADS7-V2 by following the example software setup procedure from the user guide:  AD917x-FMC-EBZ Evaluation Board User Guide [Analog Devices Wiki]

I have the ADS7-V2 connected to power with its 12V, 5A power supply, and connected to my computer via USB.

The AD9174 is connected to the ADS7-V2 and is also connected to the computer via USB cable.

I am following the steps from the example software setup but am not getting the Links 0 and 1 to show with the green check mark after hitting “Stop”, then “Download”, then “Resync”, then “Play” in DPGDownloader. The links don’t go high, and the Serial Line Rate on the GUI does not read 9.8304Gbps as you can see in the following image:

 

This is how ACE is being set up:

 

 

I have gone through the steps multiple times with the same result. I have reset everything and power cycled the boards and I get the same thing. I have downloaded the AD9172 Plug-in in ACE as well.

Any help would be greatly appreciated.

Thanks.