AD9102 Time from the start of pattern generation to the output

Let me ask you about the time from when TRIGGER is set to Low in DDS until the waveform is output.

Let me ask you about the time from when PATTERN_DELAY VALUE = 0, is set to Low until the waveform is output.

Q1: When PATTERN_DELAY VALUE = 0, START_DELAY = 0 is set
The delay until output is
Is it 96ns of "Trigger to Output Delay, fDAC = 180 MSPS2" in the data sheet table 6?

Q2 Does this 96ns depend on the speed of fDAC?