Post Go back to editing

DAC AD9172 Mode selection & Register configuration

My DAC requirements are
1. Single link mode
2. L : 8
3. M : 2
4. F : 1
5. S : 2
6. NP : 16
7. N : 16
8. K : 32
9 HD :1
10. SUBCLASS 1

My sampling frequency is 2.94912 GHz . From this i have calculated the Lane rate i.e. 14.7456Gbps .
datapath interpolation and main path interpolation are (x1) . I am Using Ultra scale FPGA which consists GTH transceiver of 16.3 Gbps lane rate capability.
i am using Direct clock source insted of internal PLL.

I have dought in my JESD mode selection and what are the registers to configure for the JESD communication.

From start up sequence i have followed
1. power up sequence
2. DAC PLL configuration first three registers
--> 0x095 -- 0x01
--> 0x790 -- 0xFF
--> 0x791 -- 0xFF
3. JESD Mode set up registers for single link.
4. JESD SERDES Required interface setup.
5. Transport layer setup.

i have chacked the 0x281 for SERDES PLL lock . the read data is 0x01.

is this configuration is enough for JESD communication...?

When the SYNCOUT will be generated from DAC ....?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.