Post Go back to editing

Issue to get clean output of AD9707

I try to use two parallel  AD9707 on a mixed signal FPGA board for signal generation @ about 5MHz. Whilst @ the ouputs of both AD9707 a strange behavior can be noticed.

AVDD = 1.8V
DVDD = 1.8V
Diff_CLK = 65MHz
FS_ADJ 6k4 to GND
OTCM to GND
Differential Buffered Output setting using an ADA4807-4
REFIO to AD8656 to ADA4807-4

See schematics:



Register settings
Mnemonic    Addr     Bit 7     Bit 6     Bit 5     Bit 4     Bit 3     Bit 2     Bit 1     Bit 0
SPI CTL        0x00     1          0           0          0           0           0           0          0          (default)
Data              0x02     0          -            -           0           0           1           -           0
Version         0x0D     -          -            -            -           1           1           0          1
CALMEM      0x0E     -           -           0           0           -           1            0         1
MEMRDWR 0x0F     0          0           -            -           0           0            -          0           (default)

The ILA curves of the FPGA are the same as what can be measured at the DAC data inputs. e.g.:


Timing of DAC inputs related to CLK seems to be ok:

 purple depicts differential CLK input @ AD9707, yellow depicts input of LSB @ AD9707



At the DAC output respectively after the differential buffered output the curves are a way of rippling in a periodic way of 1/32 of the (full-scale) period:

 sawtooth as full scale range input - depicted is differentially measured strange behaviour @ DAC output

 sinusoidal as full scale range input - depicted is differentially measured strange behaviour @ DAC output

 sawtooth only the 5 MSBs as input - depicted is differentially measured behaviour @ DAC output

 sawtooth as input _ only the 9 LSBs as input - depicted is differentially measured strange behaviour @ DAC output

What could I have missed? Can this be smoothed without calibration in the first step?

Your help is greatly appreciated :-)
regards Matthias

Top Replies

Parents Reply Children
No Data