My customer wants to use the LTC1666 as shown in Figure 8 below.
However, I would like to use Vout in the range from 5V to 0V, so please check what to do.
Waiting for your reply.
Thank you.
LTC1666
Production
The LTC1666/LTC1667/LTC1668 are 12-/14-/16-bit, 50Msps differential current output DACs implemented on a high performance BiCMOS process with laser trimmed...
Datasheet
LTC1666 on Analog.com
My customer wants to use the LTC1666 as shown in Figure 8 below.
However, I would like to use Vout in the range from 5V to 0V, so please check what to do.
Waiting for your reply.
Thank you.
Change the 200ohms resistors to 500ohms. 10mA*500ohms = 5V
In your answer, does 200 ohms mean only RFB resistance?
Or is it 200ohm from U1(LT1812) to GND?
Or is it both resistance?
please answer about my question.
Also, can the LT1812 OPAMP power supply connect +5V to V+ and GND to V-?
Waiting for your reply.
Thank you.
Both resistors need to be changed. The LT1812 can run on a single supply, but the LTC1668 cannot.
Both resistors need to be changed. The LT1812 can run on a single supply, but the LTC1668 cannot.
The LT1812 can run on a single supply, but the LTC1668 cannot.
We will send you additional questions for cross check.
LT1812 OPAMP power supply is +5V to V+ and GND to V- as single power
However, do you mean that the LTC1666/7/8 should be powered by VDD +5V and VSS-5V dual power?
please answer about my question.
Right, the LTC1668 needs a split supply.