Post Go back to editing

AD9102 SRAM Read/Write

Hello,

I am trying to access the SRAM on an AD9102 and I’m having some issues.  All of my reads for the SRAM return 0x0000 and the other questions in this forum haven’t enabled me to successfully read/write.

When I configure the device, I set the following registers:

  • The configuration register is 0x0000
  • The start address register is 0x0000 ( At least one other question seemed imply that setting the start and stop addresses was required)
    • Verified by reading the register value back
  • The stop address register is 0xFFF0
    • Verified by reading the register value back

When I try to load 4 memory locations into the device, I’m use the following sequence:

  1. 0x801E 0x0000 = Get PAT_STATUS
    1. Reply 0x0000 0x0000
  2. 0x001E 0x0004 = Set MEM_ACCESS in PAT_STATUS
  3. 0x001D 0x0001 = Set UPDATE in RAM_UPDATE
  4. 0x801E 0x0000 = Get PAT_STATUS
    1. Reply 0x0000 0x0004
  5. 0x6000 0x0000 0xAAB0 0x5560 0x0010 = Write 2’s compliment, left justified of 0x0000, 0x5550, 0xAAA0, 0xFFF0 into SRAM starting location 0x6000

This seems to be correct and I can clearly see this going into the device using a logic analyzer.  However, when I try to read the memory, I only receive 0’s.  I am using the following sequence to read:

  1. 0x801E 0x0000 = Get PAT_STATUS
    1. Reply 0x0000 0x0004
  2. 0x001E 0x000C = Set MEM_ACCESS in PAT_STATUS
  3. 0x001D 0x0001 = Set UPDATE in RAM_UPDATE
  4. 0x801E 0x0000 = Get PAT_STATUS
    1. Reply 0x0000 0x000C
  5. 0xE000 0x0000 0x0000 0x0000 0x0000 = Read SRAM Location 0x6000
    1. Reply 0x0000 0x0000 0x0000 0x0000 0x0000

My setup uses the AD9102-EBZ and I am driving the signals with an external microprocessor.  ( The SPI signals have been disconnected from the microcontroller located on the dev board.)  Since I am able to read/write the registers, I’m certain that the device is hooked up properly and the system is properly functioning, but I can’t seem to get the SRAM to respond.  Any suggestions?

Parents
  • Hi,


    Please see pseudocode below.

    1. Set initial values of IOs.
         ○ RESET - logic high
         ○ TRIGGER - logic high
         ○ CS - logic high

    2. Set SPI frequency and mode.
         ○ Clock is logic low when idle or leads with a rising edge and trails with a falling edge.
         ○ Data logic level should be valid during the clock rising edge and before the clock falling edge.

    3. Pulse RESET to logic low then high to reset register values.

    4. Proceed with register read or write. (AD9102: page 18, AD9106: pages 22-23 of datasheet)
         a. If loading a pattern from SRAM, write data on SRAM registers first. (AD9102: page 23, AD9106: page 27 of datasheet)
              i. To write data: Enable MEM_ACCESS bit in 0x1E register. Write left-justified data to SRAM registers, 0x6000 to 0x6FFF. Disable MEM_ACCESS bit.
              ii. To read data: Enable BUF_READ and MEM_ACCESS bits in 0x1E register. After reading data from SRAM registers, disable BUF_READ and MEM_ACCESS bits.
         b. Write on SPI registers. Update last bits of registers 0x1E (RUN bit) and 0x1D (RAMUPDATE bit) at the end of the write sequence.


    Best regards,
    Shine

  • Hello Shine, thank you for the assistance.

    Following these steps, I am still unable to write and then read to the SRAM.

    1. State of I/Os: RESET_B is HIGH (+3.325V); TRIGGER_B is LOW (+0.001V); CSB is HIGH (+3.341V)
      1. Verified with a calibrated multimeter probing the actual dev board
    2. SPI Frequency and Mode
      1. Frequency is 714kHz (1.4us)
      2. CS is Active Low
      3. Clock is Rising Edge
    3. Pulse Reset Low then High
      1. I press and hold S1 for ~1second
    4. Write SRAM Data
      1. Read PAT_STATUS = 0x0000 (Checking for RUN Bit)
      2. Read PAT_STATUS = 0x0000 (Getting Current Register Status)
      3. Write PAT_STATUS MEM_ACCESS = 0x001E 0x0004
      4. Write RAM_UPDATE UPDATE = 0x001D 0x0001
      5. Write SRAM DATA = 0x6000 0x0000 0xAAB0 0x5560 0x0010
      6. Read PAT_STATUS = 0x0004 (Checking for RUN Bit)
      7. Read PAT_STATUS = 0x0004 (Getting Current Register Status)
      8. Write PAT_STATUS = 0x001E 0x0000
    5. Read SRAM Data
      1. Read PAT_STATUS = 0x0000 (Checking for RUN Bit)
      2. Read PAT_STATUS = 0x0000 (Getting Current Register Status)
      3. Write PAT_STATUS BUF_READ and MEM_ACCESS = 0x001E 0x000C
      4. Write RAM_UPDATE UPDATE = 0x001D 0x0001
      5. Read SRAM DATA =
        1. MOSI: 0xE000 0x0000 0x0000 0x0000 0x0000
        2. MISO: 0x0000 0x0000 0x0000 0x0000 0x0000
          1. MISO Should be 0x0000 0x0000 0xAAB0 0x5560 0x0010
      6. Read PAT_STATUS = 0x000C (Checking for RUN Bit)
      7. Read PAT_STATUS = 0x000C (Getting Current Register Status)
      8. Write PAT_STATUS = 0x001E 0x0000

    If it is helpful, I can provide CVS files that show the exact timing of the signals.

Reply
  • Hello Shine, thank you for the assistance.

    Following these steps, I am still unable to write and then read to the SRAM.

    1. State of I/Os: RESET_B is HIGH (+3.325V); TRIGGER_B is LOW (+0.001V); CSB is HIGH (+3.341V)
      1. Verified with a calibrated multimeter probing the actual dev board
    2. SPI Frequency and Mode
      1. Frequency is 714kHz (1.4us)
      2. CS is Active Low
      3. Clock is Rising Edge
    3. Pulse Reset Low then High
      1. I press and hold S1 for ~1second
    4. Write SRAM Data
      1. Read PAT_STATUS = 0x0000 (Checking for RUN Bit)
      2. Read PAT_STATUS = 0x0000 (Getting Current Register Status)
      3. Write PAT_STATUS MEM_ACCESS = 0x001E 0x0004
      4. Write RAM_UPDATE UPDATE = 0x001D 0x0001
      5. Write SRAM DATA = 0x6000 0x0000 0xAAB0 0x5560 0x0010
      6. Read PAT_STATUS = 0x0004 (Checking for RUN Bit)
      7. Read PAT_STATUS = 0x0004 (Getting Current Register Status)
      8. Write PAT_STATUS = 0x001E 0x0000
    5. Read SRAM Data
      1. Read PAT_STATUS = 0x0000 (Checking for RUN Bit)
      2. Read PAT_STATUS = 0x0000 (Getting Current Register Status)
      3. Write PAT_STATUS BUF_READ and MEM_ACCESS = 0x001E 0x000C
      4. Write RAM_UPDATE UPDATE = 0x001D 0x0001
      5. Read SRAM DATA =
        1. MOSI: 0xE000 0x0000 0x0000 0x0000 0x0000
        2. MISO: 0x0000 0x0000 0x0000 0x0000 0x0000
          1. MISO Should be 0x0000 0x0000 0xAAB0 0x5560 0x0010
      6. Read PAT_STATUS = 0x000C (Checking for RUN Bit)
      7. Read PAT_STATUS = 0x000C (Getting Current Register Status)
      8. Write PAT_STATUS = 0x001E 0x0000

    If it is helpful, I can provide CVS files that show the exact timing of the signals.

Children