Post Go back to editing

AD9764 output

Hi

I have designed a DAQ borad including AD9764, AD6644 and it communicates with Xilinx Spartan 3AN FPGA through FX2 expansion connector.

As indicated in the attachments we can see the input&output connections and the clock signal (which is RC filtered version of Clockin at 16MHz coming from the FPGA) . I am wondering why i am getting the same voltages at the IOUTA and OUTB nodes at the AD9764 output (simply 0 or 20mV at the output of AD9631 opamp ) although I apply the code "00000001111111" from the FPGA. I checked the DAC inputs and see that they are as the FPGA output.  Is it about the AD9764 or the AD9631 opamp or the noise level?

I will appreciate any help .

Thank you very much

HIDIR

attachments.zip
Parents
  • Hi Mr. Larry Welchusa

    Thank you very much for your help

    I attached the schematic pdf file. I can also send the layout files' pictures.

    In addition to the schematic i have made two differences in the layout. The first one is adding two capacitors for obtaining CLOCK signal from the incoming CLOCKIN signal (i added 100nF capacitors in serial with the AD9764 and 74LCX574(D flip flop at the AD6644 output) clock inputs ). Thus the 98th pin of the Hirose FX2 connector is then CLOCKIN. https://ez.analog.com/servlet/JiveServlet/download/59065-11376/AD9764clock.jpg

    The second is the addition of RC parallel pairs at the AD9764 IOUT pins . ez.analog.com/.../DiffAmpConfig.JPG

    Also i do not think that there is a current sourcing lack in the supplies . The AVCC=5V and it sources 315 mA (6.5V and 350mA limited by the Agilent DC power supply). The DVDD=3.3V sources 116mA (for all high input of AD9764) and it is 5.5V and 150mA limited. The AVEE=-5V sources 20 to 40 mA (only for the OPAMPs) and 8V and 100mA limited. The Vref=2.4V (only for the AD6644 and AD8138) and limited to 4.4V and 100mA (sources no current when the AVCC is connected).

    I use Tektronix oscilloscope to observe the signals. I use Xilinx SPARTAN 3AN FPGA kit (the connection to the DAQ card is established using Hirose FX2 connector).

    Thank you very much.

    boardHIDIR.pdf
Reply
  • Hi Mr. Larry Welchusa

    Thank you very much for your help

    I attached the schematic pdf file. I can also send the layout files' pictures.

    In addition to the schematic i have made two differences in the layout. The first one is adding two capacitors for obtaining CLOCK signal from the incoming CLOCKIN signal (i added 100nF capacitors in serial with the AD9764 and 74LCX574(D flip flop at the AD6644 output) clock inputs ). Thus the 98th pin of the Hirose FX2 connector is then CLOCKIN. https://ez.analog.com/servlet/JiveServlet/download/59065-11376/AD9764clock.jpg

    The second is the addition of RC parallel pairs at the AD9764 IOUT pins . ez.analog.com/.../DiffAmpConfig.JPG

    Also i do not think that there is a current sourcing lack in the supplies . The AVCC=5V and it sources 315 mA (6.5V and 350mA limited by the Agilent DC power supply). The DVDD=3.3V sources 116mA (for all high input of AD9764) and it is 5.5V and 150mA limited. The AVEE=-5V sources 20 to 40 mA (only for the OPAMPs) and 8V and 100mA limited. The Vref=2.4V (only for the AD6644 and AD8138) and limited to 4.4V and 100mA (sources no current when the AVCC is connected).

    I use Tektronix oscilloscope to observe the signals. I use Xilinx SPARTAN 3AN FPGA kit (the connection to the DAQ card is established using Hirose FX2 connector).

    Thank you very much.

    boardHIDIR.pdf
Children
No Data