Hi,
Considering the AD9764 evaluation board which is shipped with transformer coupled output option, the DAC output current is 2 to 20 mA, the output voltage compliance range is -1 to 1.25V (calculated from dac transfer fuctıon as : +-0.96V),the minicircuits' T1-1T transformer (http://217.34.103.131/pdfs/T1-1T-KK81.pdf)
I am getting about 100mV pk-pk output from the secondary side with no load.
Do you have any suggestion about the load that can be connected in parallel to the transformer secondary winding output ?
Thanks
HIDIR