AD9102
Production
The AD9102 TxDAC and waveform generator is a high performance digital-to-analog converter (DAC) integrating on-chip pattern memory for complex waveform...
Datasheet
AD9102 on Analog.com
I’m using AD9102, I write and read in all register but I haven't output signal.
What is the minimum registers configuration for generate a signal?
Can it work without calibration?
In attachment the schematic.
Regards.
Valentino
Hello Larry,
Thanks for getting back to me so fast.
The simplest waveform I want to generate is a swept square wave.
So Ram [0] = 0x7FFF (-ve min)
Ram [1] = 0x8000 (+ve max)
Start = 0, Stop =1, Pattern length = 2
Output directly from Ram, continuous pattern, Address counter incremented by DDS_MSB
Set DDS frequency to any value (I used 1000 Hz).
I expect a Square Wave of 500 Hz.
If this can be done, I'll be grateful!
regards
Bart
Hello Larry,
Thanks for getting back to me so fast.
The simplest waveform I want to generate is a swept square wave.
So Ram [0] = 0x7FFF (-ve min)
Ram [1] = 0x8000 (+ve max)
Start = 0, Stop =1, Pattern length = 2
Output directly from Ram, continuous pattern, Address counter incremented by DDS_MSB
Set DDS frequency to any value (I used 1000 Hz).
I expect a Square Wave of 500 Hz.
If this can be done, I'll be grateful!
regards
Bart