Post Go back to editing

AD9102 Output Signal

Thread Summary

The user is unable to generate a signal using the AD9102 despite writing and reading all registers. The solution involves setting the DDS Tuning Word source to RAM data and using the DDS MSB as the SRAM address counter clock. Additionally, the user must ensure the RAMUPDATE register is set to 1 to transfer shadow register values to active registers. The data sheet lacks clear examples and specific details, leading to confusion about the initialization sequence and register settings.
AI Generated Content

I’m using  AD9102, I write and read in all register but I haven't output signal.

What is the minimum registers configuration for generate a signal?

Can it work without calibration?

In attachment the schematic.

Regards.

Valentino

ad9102.pdf
Parents
  • 1. I've attached an example where I used the DDS MSB enable as part of generating a chirp waveform with AD9106. The SRAM contains a list of DDS tuming words. The result (included) is one sinewave cycle at each DDS frequency.

    2. For SAW tooth waveforms you can only adjust teh number of samples per step.

    I hope thuis helps.

    Thanks,

    Larry

    chirp.zip
Reply
  • 1. I've attached an example where I used the DDS MSB enable as part of generating a chirp waveform with AD9106. The SRAM contains a list of DDS tuming words. The result (included) is one sinewave cycle at each DDS frequency.

    2. For SAW tooth waveforms you can only adjust teh number of samples per step.

    I hope thuis helps.

    Thanks,

    Larry

    chirp.zip
Children