If, instead of using high temperature to solder the component, I use a low temperature conductive epoxy (55C) to bond it. Do I still need to bake the component at 150C for 24 hours?
\Lego
AD5346
Production
The AD5346 / AD5347Â / AD5348Â are octal 8-, 10-, and 12- bit DACs, operating from a 2.5 V to 5.5 V supply. These devices incorporate an on-chip output...
Datasheet
AD5346 on Analog.com
If, instead of using high temperature to solder the component, I use a low temperature conductive epoxy (55C) to bond it. Do I still need to bake the component at 150C for 24 hours?
\Lego
Hi,
If you are not heat up the part (>150c), you dont need to bake it before.
Hi,
If you are not heat up the part (>150c), you dont need to bake it before.