Post Go back to editing

AD9102 OUTPUT SWEEPING SINE WAVE

Thread Summary

The user wants to output a sweeping sine frequency in TTL voltage levels using the AD9102. The final answer suggests using an amplifier to convert the AD9102's current output (up to 8mA, -0.5V to +1.0V compliance) to TTL levels. The SRAM can store tuning words for the on-chip DDS, with a tuning resolution of 10.8Hz at 180MHz CLKP/CLKN. The pattern is repeated at 50Hz, and 10 cycles are needed per frequency point from 20kHz to 30kHz in 1kHz steps.
AI Generated Content

hi.

I want to output sweeping sine frequency in TTL voltage levle using AD9102. The datasheet is so vague that i can just output constant voltage.Is there anyone who can help me fix this:

Output frequency range: 20kHz to 30kHz, 1kHz step;

Number of cycles:10 cycles/frequency point.

                                                                            Best regards!