Post Go back to editing

AD9106 external Vref gain drift?

Thread Summary

The user is concerned about the 267 PPM gain drift and 160 PPM/°C internal reference drift of the AD9106. The final answer explains that to recalculate gain drift with an external reference, subtract the internal reference voltage drift from the gain drift, then add the external reference's drift. The user plans to use a fixed, low-temperature coefficient resistor to improve stability.
AI Generated Content

So I thought the AD9106 was the perfect solution to my problem but now I realized that it has a fatal flaw, the 267 PPM gain drift, specified with the rather drifty internal reference, which has a 160PPM / degree C drift.

If a very stable external reference is used, how is gain drift re-calculated? I hope that maybe the datasheet writers tested the drift with a poor tempco Rset resistor as well.... (I could use a vishay foil here if it helps!)

I was hoping to knock it down an order of magnitude to make it usable..

Thank you.

  • Hi.

    I have moved this thread to the High-Speed DAC community. Someone should be able to assist you here.

    Best Regards,

    Sittie

  • Hi -

    In charaterizing the AD9106 temp drift, the on-chip reference drift and gain (IOUTFS) drift with the internal reference in use were measured fro a population of devices. To calculate the IOUTFS temp drift when using an off chip reference calculate GAIN Temp Drift - Internal Reference Voltage Temp Drif. This number is the temp drift of everything except the reference. Add the temp drift of your externalk reference to this number to get the IOUTFS temp drift with external reference.

    Thanks,

    Larry 

  • Ok. But do you know if disabling the internal Rset resistors has a significant impact on drift? I assume that the chips were tested using the on-board adjustable resistors, which may have poor tempco in comparison to external foil resistors... especially if they are used in rheostat mode like the block diagram implies, in most manufacturer data-sheets I see that rheostat mode digipots have a temp co at best of 30-100 ppm. I planned on disabling these and using a fixed very low temperature coefficent resistor.

    Thank you for your time and response.