Post Go back to editing

Single-port mode of dual DAC

I have a question about single-port mode of dual DAC.
Could you  show me the answer of following problem.

 

For example AD9741,AD9743,AD9745,AD9746,AD9747,
In the case of using these dual DACs with single-port mode and only DAC1,
how should I do IQSEL pin ?

 

1. Open with setting ONEPORT = 0
    That is, as we select dual-port mode, the IQSEL input is ignored.
2. Connect it to VDD
    Always DAC1 is selected.
3. I/Q frame signal of FPGA
4. Other

 

I am waiting for your reply.

 

Best regards,