Post Go back to editing

AD9146 power-up time

Hello!
I have a few questions about AD9146 power-up time.
This DAC has 260 ms power-up time.
Why it's so much?
Is it independent time (of operating mode, operating conditions, etc)?
Can I reduce this time by DAC PLL turn off?

Parents
  • The specified power-up time includes the time to fully charge the decoupling cap on the REFIO pin upon power up. The device will not be fully functional before the REFIO pin reaches 1.2V (bandgap voltage). This is a "cold" start.

    The power up time is much shorter in a "warm" start as the bandgap voltage is already at 1.2V. A software reset is an example of a "warm" start. It should be less than 1ms depending on the clock rate.

Reply
  • The specified power-up time includes the time to fully charge the decoupling cap on the REFIO pin upon power up. The device will not be fully functional before the REFIO pin reaches 1.2V (bandgap voltage). This is a "cold" start.

    The power up time is much shorter in a "warm" start as the bandgap voltage is already at 1.2V. A software reset is an example of a "warm" start. It should be less than 1ms depending on the clock rate.

Children
No Data