Post Go back to editing

AD9102 - Differential To Single Ended Voltage

Thread Summary

The user encountered signal distortion when using the ADA4817 opamp to convert a 1ms voltage ramp from the AD9102 DAC to a single-ended output without a negative supply. The solution was to either use a negative supply or sum in a DC offset at the amplifier input. The user confirmed that adding a negative supply resolved the issue. Additional questions were raised about the need for a buffer between the DAC and opamp, the nature of the AD9102's differential current outputs, and the interpretation of the output compliance voltage specification.
AI Generated Content

We are attempting to use the following circuit to produce a single ended voltage ramp on the output:

The circuit is based on the circuit used in the AD9102 eval board, except that there is no negative supply (-Vs is tied to ground instead).  

The AD9102 is generating a 1ms ramp that looks fine when probed directly at the outputs of the AD9102, but then appears distorted at the output of the ADA4817.  It seems as though the AD4817 is integrating the signal.  This distortion/integration occurs with or without the feedback capacitor C17 installed. 

Any suggestions on what might be happening?

Thanks

JCole