Post Go back to editing

AD9106/AD9102 clock issue

Thread Summary

The user experienced SPI communication failure on the AD9106 when the DAC clock (TI CDC421 156 MHz LVPECL) was enabled. The issue was resolved by using an LVDS clock (IDT ICS844021-01 at 166.66 MHz) and powering the AD9106 at 1.8 V, which corrected the CLDO voltage from 1.4 V to 1.8 V.
AI Generated Content

I have a really strange issue with SPI communication on the AD9106.

When I disable my DAC clock (TI CDC421 156 MHz LVPECL), SPI communication (330 kHz) works great, but when I turn the DAC clock on, I lose SPI communication-- I can no longer read from the registers.

How could the DAC clock affect SPI communication?

Perhaps I'm not terminating my DAC clock or AC-coupling it properly, but I think it's fine:

I see the common mode voltage properly sitting at 0.9 V and I see a 500 mV peak-to-peak swing from CLKP to CLKN

One thought is that there might be a setup time issue that arises with using the faster clock.

Or, if I'm not terminating it correctly, there's some sort of over-current issue?

I'd really appreciate some insight into what might be going on.


Pete

Parents
  • Thanks, Larry. I think there's still something strange going on with the DAC clock.

    SPI works great if the DAC clock is disabled or if TRIGGER_BAR is disasserted.

    I lose SPI if I enable the DAC clock and assert TRIGGER_BAR. Then, if I disassert TRIGGER_BAR, SPI is not restored, but if I turn off the DAC clock, SPI comes back. So strange!

    Do you have any insight as to why this would happen? I seriously think it's a clock issue. I'm trying to use the clock circuit in the picture above. I'll probably end up trying to use a different clock, but I'd really like to know why/if this one is fouling things up.


    Pete

Reply
  • Thanks, Larry. I think there's still something strange going on with the DAC clock.

    SPI works great if the DAC clock is disabled or if TRIGGER_BAR is disasserted.

    I lose SPI if I enable the DAC clock and assert TRIGGER_BAR. Then, if I disassert TRIGGER_BAR, SPI is not restored, but if I turn off the DAC clock, SPI comes back. So strange!

    Do you have any insight as to why this would happen? I seriously think it's a clock issue. I'm trying to use the clock circuit in the picture above. I'll probably end up trying to use a different clock, but I'd really like to know why/if this one is fouling things up.


    Pete

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.