Post Go back to editing

AD9102/6 frequency change

hello

How fast can the output frequency change between two fixed frequencies in the AD9102/6?

Is it as low as <50nSec?

Parents
  • Hi Biao

    Thanks for the reply.

    Actually, any two frequencies.

    I would assume that the worst case is when f1 is close to DC & f2 is close to 90MHz (the two extremes).

    Yes I know that these can be stored in SRAM then played continuously, that's why I've thought abouth the device in the first place.

    BR,

    Alom

Reply
  • Hi Biao

    Thanks for the reply.

    Actually, any two frequencies.

    I would assume that the worst case is when f1 is close to DC & f2 is close to 90MHz (the two extremes).

    Yes I know that these can be stored in SRAM then played continuously, that's why I've thought abouth the device in the first place.

    BR,

    Alom

Children
No Data