hello
How fast can the output frequency change between two fixed frequencies in the AD9102/6?
Is it as low as <50nSec?
hello
How fast can the output frequency change between two fixed frequencies in the AD9102/6?
Is it as low as <50nSec?
Hi Guys
Any update?
BR,
Alon
Hi Biao
Thanks for the reply.
Actually, any two frequencies.
I would assume that the worst case is when f1 is close to DC & f2 is close to 90MHz (the two extremes).
Yes I know that these can be stored in SRAM then played continuously, that's why I've thought abouth the device in the first place.
BR,
Alom
Hi Alon,
do you have more specific requirements? like what are the two fixed frequencies? Dac clock rate?
if only two frequencies, the waveform data can be saved into SRAM then play them continuously.