Post Go back to editing

AD9746 SFDR

Hi

I have a couple of questions about AD9746.
Datasheet says that SFDR is 82, 70 and 66 dBc in the individual conditions.
Do these values represent the specifications to 2nd/3rd harmonic distortion or not ?
I wonder if these values represent the specifications to the noise in the Nyquist band.
Please let me know the definition of SFDR in the datasheet of AD9746.

Best Regards

Parents
  • The spurs sown I the attached spectrum capture are not harmonics caused by the AD9746. They may be due to a timing problem on the input data and clock. Setup and hold times between CLKP/CLKN and P1D and P2D busses are worth looking at. As well as the amplitude of CLKP/CLKN relative to table 5 in the data sheet.

    Thanks

Reply
  • The spurs sown I the attached spectrum capture are not harmonics caused by the AD9746. They may be due to a timing problem on the input data and clock. Setup and hold times between CLKP/CLKN and P1D and P2D busses are worth looking at. As well as the amplitude of CLKP/CLKN relative to table 5 in the data sheet.

    Thanks

Children
No Data