Post Go back to editing

AD9778 Input Clock Harmonics

Hiya,

I'm using an AD9778 and AD9779, both on custom PCBs. They are both running with the default register settings (with the exception of register 0 set to 0x80 to enable the bi-directional serial interface). As such the internal PLL is disabled, so too is interpolation. My reference clock and data rate is 160 MHz. Unfortunately I am seeing very high (-10 dBm) harmonics of the input clock on the output of the device at 320 and 640 MHz.

Has anyone else had this problem?

Thanks

Parents Reply Children
No Data