Post Go back to editing

AD9106 waveform synchronisation

Thread Summary

The user inquired about synchronizing multiple AD9106 devices using clock signals. The final answer indicated that the question was assumed to be answered offline or with a multi-part answer, and the thread is now closed. An accompanying answer suggested that pattern generation can be synchronized using the trigger input signal.
AI Generated Content

AD9016 waveform synchronisation

Is it possible to synchronise multiple AD9106 devices in a system using just the clock signals or does it require special software control to do so?

Thanks

Parents Reply Children
No Data