Post Go back to editing

AD9106 sine output and tuning words

Hello,

Is it possible to output prestored sinewaves with the frequency tuning words coming from the RAM and the clock for the RAM address coming from DDSx MSB?

Parents
  • I'm a little bit confused here - on page 26 of the datasheet the tuning word is formed with the combination of DDSTW_MSB bits and RAM. DDSTW_MSB is DDS_TW32 register @ Address 0x3E. In the description of the TW_RAM_CONFIG Register the tuning word is formed with DDS1TW:RAM
    Which register is DDS1TW? DDS_TW1 @ Address 0x3F or DDS_TW32 @ Address 0x3E?

Reply
  • I'm a little bit confused here - on page 26 of the datasheet the tuning word is formed with the combination of DDSTW_MSB bits and RAM. DDSTW_MSB is DDS_TW32 register @ Address 0x3E. In the description of the TW_RAM_CONFIG Register the tuning word is formed with DDS1TW:RAM
    Which register is DDS1TW? DDS_TW1 @ Address 0x3F or DDS_TW32 @ Address 0x3E?

Children
No Data