Post Go back to editing

AD9102 output signal quality and filtering

Hello together,

at the moment we are busy designing a wide band application using AD9102 produducing a permananet sine wave. With the help of some forum post device now is running.

Setup is fine and frequency and amplitude can easily be adjusted. Requierement is to build a adjustable Sine wave which frequency can be trimed from 4kHz up to 35MHz.

Bassically this works but when I look at the output waveform I am little bit confused concerning output signal quality. Although LVDS is running with 180MHz output of the DDS does not really look like a good sine. Even when a 11,25 MHz sine wave is configuredn it you can easily see quite big resulotion steps. Steps can also be recognized very clear when frequency is set to 1,8 MHz although step size is smaller.

But we need a more smoother output signal where the single steps are not that clear to see.

We thought when using AD9102 with integrated DDS option that there are some signal filter elements are integrated to make a good output signal without having the need to filter externally. This is what we normaly expect when using a DDS and other DDS behave like this.

Of course I can use an external filter for smoothing but before I do this my question:

Is there anything else we have to take into consideration when configuring the device? Is there any chance to influence output quality of the signal or to advice DDS core to make smaller and more steps?

Thanks in advance

Christian

Parents
  • Hi,

    sorry for  the delay, I was busy with other projects but now I can come back to that issue.

    See, but exactly that is the issue I don't understand. If I install a passive post filter there is no active source bringing the voltage at the corresponding pins to a voltge level higher as values mentioned in the table.

    There is no active source installed in that case.

    Or is that a problem to use a 5th order butterworth filter or higher?  Because I recognize that application is working with a 3rd order filter but for higher frequencies this filter is not steep enough to filter our signal to a sine wive withouth high frequency noise.

    Or would you suggest to use another DDS with a higher clock rate to fullfill our requirement withouth having to use a high order output filter to get a 35MHz sine wave?

    Any hint is very welcomed

    Christian

Reply
  • Hi,

    sorry for  the delay, I was busy with other projects but now I can come back to that issue.

    See, but exactly that is the issue I don't understand. If I install a passive post filter there is no active source bringing the voltage at the corresponding pins to a voltge level higher as values mentioned in the table.

    There is no active source installed in that case.

    Or is that a problem to use a 5th order butterworth filter or higher?  Because I recognize that application is working with a 3rd order filter but for higher frequencies this filter is not steep enough to filter our signal to a sine wive withouth high frequency noise.

    Or would you suggest to use another DDS with a higher clock rate to fullfill our requirement withouth having to use a high order output filter to get a 35MHz sine wave?

    Any hint is very welcomed

    Christian

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.