Hi,
Can I use the current output of current sourcing DACs, like AD9707, AD9744 or AD9777, for high frequency (1MHz) bio-impedance measurement ?
We often used I-V conversion circuit after DAC to convert the output to buffered voltages, and then design a VCCS (for example, howland circuit) for current output. So, I wonder if the current output of DAC (after anti-aliasing filtering) can be used directly as a current source for bio-impedance measurement.
Thanks!