Post Go back to editing

Which should I connect REFLO of AD9744 to ? ACOM or AVDD ?

Hi, in the datasheet of AD9744, it states that REFLO should be connected to ACOM for both internal and external reference operation modes. However in the reference designs (SOIC), it says that if you want to use external REFIO, you should tie REFLO to AVDD. I search some other documents such as AD9708 and AD9754, they all say that if you want to use external REFIO, you should tie REFLO to AVDD to disable internal VREF.

So, for AD9744, if I want to use external VREF, where should I connect REFLO to ? AVDD or ACOM ?

Thanks!

Parents
  • Thanks! I think the reference schematic of AD9744 should be updated accordingly  I found that Agilent 33220A (which uses AD9744) tied REFLO to AVDD, is there any drawbacks in doing so ? should I leave a backup plan where REFLO are tied to AGND via a 0Ohm resistor and a DNP resistor pulled to AVDD?

Reply
  • Thanks! I think the reference schematic of AD9744 should be updated accordingly  I found that Agilent 33220A (which uses AD9744) tied REFLO to AVDD, is there any drawbacks in doing so ? should I leave a backup plan where REFLO are tied to AGND via a 0Ohm resistor and a DNP resistor pulled to AVDD?

Children
No Data