Post Go back to editing

AD9106 internal Rset range and values

Thread Summary

The user asked about the value, range, and step size of the internal resistors (RSET) for the AD9106 DACs. The support engineer confirmed that at reset, each DACx_RSET is set to 0x0A, which programs the resistor to 8kOhm. The range is 0 to 16kOhm with a step size of 800Ohm, and the full-scale output current (IOUTFS) is 4mA with a 1.0V REFIO.
AI Generated Content

The AD9106 has internal resistors (RSET) to adjust the reference current for each of the four DAC’s.

The block diagram shows 16kOhm adjustable resistors connected internally to FSADJ1/2/3/4

And the FSADJx registers (0x09, 0x0A, 0x0B, 0x0C) show that they are 5 bit value.

What is the value, range,  and step size for those internal resistors.