Sync two AD9963

Hi, in my application, I want to use 2pcs of AD9963 on one board to get a Quad channel ADC inputs + Quad Channel DAC outputs, is it possible to sync these two AD9963 by bypassing the DLLs? Drive two 9963's CLK with a CLK distribution chip instead, will this make these two 9963s' 4 ADCs and 4 DACs have no phase differ? 

And, will the 2× decimating low-pass filter affect the 4 ADCs' sync? 

Thanks you! 

Frank

  • 0
    •  Analog Employees 
    on Sep 2, 2017 12:22 AM

    I'm going through open issues and found this one didn't get answered. The part wasn't designed with multi-device sync as a requirement, so there are likely instances whereby the two devices may become out of sync, even when measures are taken externally to do synchronization of the two.