Post Go back to editing

AD9102: help with generator random waveform

Thread Summary

The user is having trouble setting up the AD9102 to output a random waveform from SRAM. The final answer clarifies that SRAM addresses are 16-bit, with the 12-bit Start_ADDR and Stop_ADDR occupying the lower 12 bits. The solution includes a C code example and a register values file for generating a Gaussian waveform from SRAM. The accompanying answers provide additional configuration steps and a reference to the AD9106 EVB schematic for further guidance.
AI Generated Content

Hi all;

I'm having difficulty setting up the AD9102 to output random waveform from the SRAM (it does not work at all!, And we have already generator SIN_WAVE and SAW_WAVE). Here are several question during datasheet;

1.About Start_ADDR & Stop_ADDR in generator random waveform;

   As we known, the ADDR of SRAM is 16bit(0x6000~0x6fff) but Start_ADDR with only 12-bit available,so does it means Start_ADDR occupy 12LSB of the SRAM ADDR;(i've gotten that the DAC_output occupy 12MSB of SRAM_ADDR);

2. Here are the C code from the AD9102: help with /TRIGGER programming  

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60001000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60010000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60022000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60030000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60043000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60050000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60064000);

SPIbusSet(SPIBUS_DEV_AOM_DAC,0x60070000);

what surprising me most is how can it generator random waveform! From date sheet, we were known[15:12]is reserved!!

3.Is there any different  in Configuring the some  basic SFR (like SPI_configure) between the generator SIN_WAV and random  waveform .

4. Our MCU is the basic 8051(TTL-level instead of 3.3V). We wonder it will bring any side_effect to ad9102?

I find the documentation very confusing, so thanks for any input you might have on this.

Thanks!

Mayer

 

 

  • Hi -

    I've attached the register values file and an SRAM vector for an example that generates a Gaussian waveform from SRAM. SRAM addresses are justified as shown below. A new rev A datasheet is in process that makes this update. 

    Thanks

    0x6000 to 0x6FFF

    SRAM_DATA

    [15:8]

     

    SRAM_DATA[15:8]

    N/A

    RW

     

    [7:0]

    SRAM_DATA[7:4]

    RESERVED

     

     

    attachments.zip
  • Hi

    My schematic is below :

     

    But my DAC (AD9102) not work.

    Please Help me.

    My code is in attache.

      0x00000000); /* SPICONFIG */

      0x000101C7); /* POWERCONFIG */

      0x00020000); /* CLOCKCONFIG */

      0x00030000); /* REFADJ */

      0x00070000); /* DACAGAIN */

      0x00080000); /* DACRANGE */

      0x000C000A); /* DACRSET */

      0x001E0000); /* PAT_STATUS - STOP */

      0x001D0001); /* RAMUPDATE */

     

      0x001F0001); /* PAT_TYPE - finite */

      0x00200000); /* PATTERN_DLY */

      0x00258000); /* DACDOF - max negative */

      0x00270000); /* WAV_CONFIG - SRAM values */

      0x00280111); /* PAT_TIMEBASE */

      0x0029000A); /* PAT_PERIOD */

      0x002B0001); /* DAC_PAT - 1 time */

      0x002C0001); /* DOUT_START */

      0x002D0010); /* DOUT_CONFIG */

      0x00318000); /* DAC_CST */

      0x00354000); /* DAC_DGAIN 0x400=1x */

      0x00370007); /* SAW_CONFIG */

      0x003E0100); /* DDS_TW32 */

      0x003F0000); /* DDS_TW1 */

      0x00430000); /* DDS_PW */

      0x00440002); /* TRIG_TW_SEL */

      0x00450003); /* DDS_CONFIG */

      0x00470000); /* TW_RAM_CONFIG */

      0x005C0000); /* START_DELAY */

      0x005D0000); /* START_ADDR («4) */

      0x005E0070); /* STOP_ADDR («4) */

      0x005F0001); /* DDS_CYC */

      0x001D0001); /* RAMUPDATE */

     

      0x001E0004); /* PAT_STATUS - MEM_ACCESS ON */

      0x001D0001); /* RAMUPDATE */

     

     ,0x60001000);

     ,0x60010000);

     ,0x60022000);

     ,0x60030000);

     ,0x60043000);

     ,0x60050000);

     ,0x60064000);

     ,0x60070000);

     

      0x001E0000); /* PAT_STATUS - MEM_ACCESS OFF */

      0x001D0001); /* RAMUPDATE */

      0x001E0001); /* PAT_STATUS - RUN */

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.