AD9162 Inconsistent JESD Link Initialization

I am using the AD9162-FMCC-EBZ eval board with the Xilinx KCU105 eval board. The JESD link fails to establish about 90% of the time after initialization and setup, but once it establishes, I get the DAC output I expect. When the link fails to establish, I continually "reset" the entire system (FPGA, Xilinx JESD core, and 9162) until the link establishes. I'm pretty sure all clocks are setup successfully; my sense is that something in the JESD link is marginal.

My startup and initialization process (on power-on and post-reset) is the following:

1. Initialize the onboard ADF4355 to output 5760 MHz. I do not believe this step ever fails.

2. Initialize the onboard AD9508. I do not believe this step ever fails.

3. Initialize the JESD FPGA core. This step involves writing registers to the core and issuing a soft reset. I do not continue past this step until the JESD core informs me that it has successfully reset.

4. Initialize the AD9162. This step involves writing data to all the registers via the SPI interface. 

Here are some other data points:

1. The PLL is locking. I have an LED that lights when locked, and it is always lit

2. The values in registers 0x470, 0x471, and 0x473 contain random values when initialization and setup fails, even from retry to retry.

3. The value in register 0x472 tends to be 0xFF even during a failure to setup correctly. 

4. The values in registers 0x4B0-0x4B7 are random from reset to reset.

So here is my question: What are the most likely causes of the inconsistent initialization, and what are the fixes most likely to work? Which registers should I monitor or modify? Any advice would be appreciated.

Parents Reply Children
No Data