Post Go back to editing

DAC AD9744 evaluation board with DPG3

I have a plan to buy the DAC AD9744 EVB.(AD9744ACP-PCBZ-ND)

Q1 . Is a AD9744ACP-PCBZ-ND compatible with AD-DPG3?

I know that DPG2 has been replaced with DPG3 and DPG2's connector is same as DPG3.

But in the Analog device site of AD9744, it recommends to use with DPG2(AD-DAC-DPG-BZ).

Q2. is there any connector which is fit perfectly between AD9744ACP-PCBZ-ND(40 PIN UP HEADER MALE input) and DPG3(RA connector CMOS output) in the Analog device? Or should I use the jumper line respectively?

Q3. when I use the AD9744ACP-PCBZ-ND, do I have to inject power to the board by using power supply? is there any AC/DC converter version board(ex 220V AC / DC 5V, 9V)?

Thank you

Best regards

attachments.zip
Parents Reply Children
  • Hello Biao.H,

    I am using the xilinx board  KCU105 to generate the Baseband signal ,and need a DAC to converter the Baseband I/Q data ,then the Analog signal  is send to the IQ modulator。

    And I am looking some DACs(such as AD9122 、AD9142A),and  have some question about AD9122:

    the xilinx board  KCU105  is FMC interface,if use the AD-DAC-FMC-ADP Adaptor, the AD9122- M5375-EBZ could be matched?

    Please, could you give me a tip?

    Thank you for your support.

    Best