I have a plan to buy the DAC AD9744 EVB.(AD9744ACP-PCBZ-ND)
Q1 . Is a AD9744ACP-PCBZ-ND compatible with AD-DPG3?
I know that DPG2 has been replaced with DPG3 and DPG2's connector is same as DPG3.
But in the Analog device site of AD9744, it recommends to use with DPG2(AD-DAC-DPG-BZ).
Q2. is there any connector which is fit perfectly between AD9744ACP-PCBZ-ND(40 PIN UP HEADER MALE input) and DPG3(RA connector CMOS output) in the Analog device? Or should I use the jumper line respectively?
Q3. when I use the AD9744ACP-PCBZ-ND, do I have to inject power to the board by using power supply? is there any AC/DC converter version board(ex 220V AC / DC 5V, 9V)?
Thank you
Best regards
For AD974x low speed DAC family products, we are recommending our customer to use SDPH1 instead of DPG2/DPG3 for the evaluation. SDPH1 plus AD-DAC-FMC-ADP can fully replace the DPG2/DPG3. And it’s much cheaper and easily setup.
Some ADI precision DACs/ADCs use the same SDPH1 board.
SDPH1 - http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-sdp-h1.html#buy
AD-DAC-FMC-ADP - http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/AD-DAC-FMC.html
Hello Biao.H,
I am using the xilinx board KCU105 to generate the Baseband signal ,and need a DAC to converter the Baseband I/Q data ,then the Analog signal is send to the IQ modulator。
And I am looking some DACs(such as AD9122 、AD9142A),and have some question about AD9122:
the xilinx board KCU105 is FMC interface,if use the AD-DAC-FMC-ADP Adaptor, the AD9122- M5375-EBZ could be matched?
Please, could you give me a tip?
Thank you for your support.
Best