Hello,
I have a question about connection of AD9152 and ADL5375. Can AD9152 be connected to ADL5375 without DC cut capacitor? If yes, could you please advise me the circuit of that?
Best regards,
Akira
AD9152
Recommended for New Designs
The AD9152 is a dual, 16-bit, high dynamic range digital-to-analog converter (DAC) that provides a maximum sample rate of 2.25 GSPS, permitting a multicarrier...
Datasheet
AD9152 on Analog.com
ADL5375
Production
The ADL5375 is a broadband quadrature modulator designed for operation from 400 MHz to 6 GHz. Its excellent phase accuracy and amplitude balance enable...
Datasheet
ADL5375 on Analog.com
Hello,
I have a question about connection of AD9152 and ADL5375. Can AD9152 be connected to ADL5375 without DC cut capacitor? If yes, could you please advise me the circuit of that?
Best regards,
Akira
Hi,
AD9152 supporting 2.7V common mode output, while ADL5375 work for 0.5V or 1.5V common mode. AD9152 is good to support ADRF6720 modulator, which you can find the evb schematic as below:ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/Documents/AD9152/AD9152-ADRF6720-EBZ%20RevB%20Schematic.pdf
Regards
Patrick
Hi
There are two versions of ADRF6720. One is ADRF6720 that asks 0.5V common mode voltage and the other one is ADRF6720-27 for 2.7V common mode voltage. So ADRF6720-27 matches to AD9152. Please refer to below figure 45 for two combinations of DAC and Modulator. You can refer to ADRF6720 and ADRF6720-27 datasheet. ADRF6720/ADRF6720-27 is PLL/VCO integrated Modulator supporting upto about 3GHz. You can interface AD9152 to either ADL5373-05/15 with some additional circuit like a level shifter. I copy examples at ac coupling case.
Thanks
Tony
Hi Tony,
Thank you for your support.
Thanks & Regards,
Akira
Hi,
I see in CN0205:

figure 1
And I think that some of the DACs suggested in the figure 1 should not be all the chips, and some of the DAC chips are not shown in the figure above. Just like adl5375's data sheet(figure 2), several DACs are not listed in the figure 1. recommendation.

figure 2 ,some DACs in the data sheet of ADL5375
And in AD9152:The full-scale output current can be programmed over a range of 4 mA to 20 mA.
https://www.analog.com/en/products/ad9152.html#product-overview
Since the ad9152 can output 20 mA of full scale current. Why can't ad9152 connect with adl5375-5.
Thanks.