Post Go back to editing

AD9712 phase mismatch between DAC0 and DAC1

Hi !

I have a problem with DAC phase of 2 DAC channels (DAC0 and DAC1) in AD917x-FMC-EBZ board (AD9172 version). In my test, I configure DAC0 out as real channel and DAC1 as imagine channel using output modular switch (AD9712 datasheet pg.60). In this case, I thinks data output of DAC0 and DAC1 must difference 90° in phase. But real output not as expected. My system setting as below.

Test condition:

  •      LINK LAYER
    •       JESD204B, Subclass1. SYSREF ON. AC mode
    •       JESD mode 1: L=2, M= 4, F=4, N=16. SCR off.
    •       Lane Rate : 10.240 GBPS
  •      DATA PATH:
    •       Input:
      •       Input data rate : 256 MHz
      •       Baseband Frequency : 0
    •      Channel path
      •      Channel interpolation : 6
      •      Channel NCO frequency : 100MHz to 300 MHz
      •      NCO integer mode.
      •      Phase offset : 0
      •      Input Gain :
        •      Channel 1: 2048
        •      Channel 2: 0
        •      Channel 3: 0
        •      Channel 4: 2048
        •      Channel 5: 0
        •      Channel 6: 0
      •      MAIN PATH :
        •     Interpolation : 8
        •      Modulator Switch : Mode2 (DAC0_I to DAC0 core , DAC0_Q to DAC1 core)
        •      NCO frequency (not need but setting to 100MHz)
      •      MESASURE equipment:
        •      Oscilloscope RTM2054 of ROHDE and SCHWARS ( 5 GSPs – 500 MHz)
        •      Probe: SMA Cable with SMA to BNC adaptor, 50Ω, Frequency up to 10 GHz

Result:

Frequency (MHz)

DAC0 – DAC1 Phase difference (°)

100

51.6

200

14.06

300

-23.5

 

It seems DAC0 and DAC1 phase is changed depend on output signal frequency.

Please help me check out why phase between DAC0 and DAC is not 90°. AD9172 characteristic or analog path in EVM board or other problem.

@ I using Modulator Switch is mode 2 to ensure no mismatch between data path of DAC0 and DAC1 can affect this test.

 

Best regards!

Hoang

Parents Reply Children
No Data