AD9162 s-parameter and IBIS AMI model

Hello ,

I am requested s-parameter and IBIS AMI model for AD9162BBCA and AD9162BBCZ from our customer.

I could not find it on the prodyct page.

About an IBIS AMI model, I found following message.

AD9162 IBIS-AMI

But AD9162 has defferent package frorm AD9144.

AMI model for AD9162 is not prepared yet ?

Do you have s-parameter to be able to provide to customer ?

Best regards,

ysuzuki

Parents
  • There is no specific IBIS-AMI model for the AD9162 DAC. We are aware of the package differences between AD9144 and AD9162 but still suggest that customers use the IBIS-AMI models for the AD9144 since the JESD core and PHY are the same design. The package model for the AD9144’s LFCSP will be “pessimistic” as compared to the BGA package for the AD9162. Basically, if you design your boards to work with the AD9144, you can be confident that it’ll work with the AD9162 since it doesn’t have as much degradation as the AD9144’s package.

    S-parameter model is not extracted for AD9162 either and I don't see it coming out anytime soon. 

Reply
  • There is no specific IBIS-AMI model for the AD9162 DAC. We are aware of the package differences between AD9144 and AD9162 but still suggest that customers use the IBIS-AMI models for the AD9144 since the JESD core and PHY are the same design. The package model for the AD9144’s LFCSP will be “pessimistic” as compared to the BGA package for the AD9162. Basically, if you design your boards to work with the AD9144, you can be confident that it’ll work with the AD9162 since it doesn’t have as much degradation as the AD9144’s package.

    S-parameter model is not extracted for AD9162 either and I don't see it coming out anytime soon. 

Children
No Data