Post Go back to editing

AD9142 design availability

The AD9142 was chosen because it had to handle 200MHz bandwidth.
1. Is it possible to set the following parameters?

fDCI = 522.24MHz (Data Rate)
fDAC = 1044.48 MHz
Interpolation: 2x
fOUT = 20MHz ~ 700MHz (Fc = 20MHz, 300MHz, 600MHz, etc)

2. There are two outputs, I and Q. Do I need to add a modulator outside?
If I'm making Jammmer signals, I can use only I signals.

Thank you.



add question!
[edited by: miney at 8:29 AM (GMT 0) on 25 Jun 2020]
Parents Reply Children