Post Go back to editing

AD9102/AD9106 delay between Trigger and Start of Generation from RAM

Hi,

I use evaluation board and try to generate signal from RAM using TRIGGER pin. But I observe 500 us delay between TRIGGER (pin 32 "1"->"0") and start of generation from RAM while datasheet say that the typical delay should be 96 ns.

Configuration for DAC1 you can see below.

As you can see all delays are zeroes. But the real delay is 524 us.

How could I get 96 ns delay between Trigger and RAM generated signal?

Best regards,
Ivan



added BR
[edited by: Ivan-Rusov at 1:16 PM (GMT 0) on 3 Sep 2019]
Parents Reply Children
No Data