Post Go back to editing

EVAL-AD9789_Internal QAM Test

Hello

My customer is considering AD9789.
Therefore I provided an evaluation board.

I followed the steps below according to the Quick Start Guide.

The operation procedure I did is as follows.
1 )5V / 2A power connection to P5 and P6
2 )CLK input from SG (2.29376 GHz_2 dB) to S1
3 )Connect spectrum analyzer to S5
4 )Connect USB Port of XP2 to PC
5 )JP9, JP10 LVDS connection for operation with 5 Internal QAM Test
6 )Check that JP setting between 2-3 pins is also set for JP7 and JP8.
7 )Turn on the power in the condition of 1 to 6 and start "AD9789.PRN" and check that STATUS is green.
8 )After pressing “load” in “AD9789.SPI” (shown below), select “AD9789_SPISettings_Int_QAM.txt” in “RUN”,
    After that, press "load" to release and "PARMNEW" is turned ON.

What I read from the data sheet is the above. Are there any steps such as deleting the procedure or setting up the GUI at the initial stage?

Evaluation board: One of the two could not confirm the waveform output.
(Some XD1 LEDs do not light green when connected to USB.)

Could you tell me about this cause?

Parents Reply Children
No Data