Hello!
We are designing a DAC module based on the AD9173. You can see the desired schematics on the picture below. We need frequencies on the output to be from 10 kHz all the way up to 6 GHz.
We understand that output of the DAC needs to be terminated with inductors to ground but lower frequencies are not possible with an inductive termination.
How could we use this DAC at lower frequencies? Is this even possible with the AD9173 and particular schematics using ADRF5024 to switch between bands? Datasheet only specifies characteristics over 100 MHz