Is it possible to create sinusoidal wave using AD9717? If so, how? The DPG Palette on the evaluation board software has an example simple sine generator, but the page is blank. Would appreciate any guidance.
Thanks
You do not need to create the vector code - there is a vector generator capability built into DPGDownloader.
On the main launch screen of DPGDownloader select "Add Generated Waveform" and there is a "single…
Yes it's possible to output a sine wave using the AD9717.
Could you send a screenshot of the DPGDownloader screen so I can understand what youmean by the palette is blank?
There is a link to download the evaluation board user guide on how to set up the software from this webpage: https://wiki.analog.com/resources/eval/dpg/eval-ad971x_ad911x?s[]=ad9717
The DPGDownloader panel should look like the attached photo if all the software is installed properly and set up as expected.
furthermore, when you do create a sine wave, would you be able to clarify what digital code in terms of units of amplitude means?
On the main launch screen of DPGDownloader select "Add Generated Waveform" and there is a "single-tone" selection you can choose.
Then you need to input your data rate and desired frequency etc as my previous screenshot shows.
thanks so much